2009-06-23 10:34 AM
multi output with ACS device plus STM32
2011-05-17 4:15 AM
Hi at all
I this my application I must connected more ACS device (24 device) for command AC motor mini-motor electrovalve all in 230Vac 50hz. I can use the stm32f101 directed powered with trasfomless a 230Vac and driver the ACS (triacs) direct from the pin on the micro? The STM32 have the certification for work in Home application? Best Regards Franco