2013-11-11 1:33 AM
Hello,
I am working with STM32F4 Discovery with FreeRTOS and summon arm tool chain.I am sending ADC data over serial Port using USB serial communication.I have write code to get ADC value in continuous conversion mode with ADC1 and channel 12.But now I have to perform Multi-channel conversion mode.So I have following Doubts please guide me regarding that1) I have refered Datasheet of STM32F4 Discovery so I came tw know that there are 16 channel but out of them how many are available..?
2)I have to connect 6 sensors to ADC channels as below ADC_1 Channel_11(PC1) ----> Sensor1 ADC_1 Channel_12(PC2) ----> Sensor2 ADC_1 Channel_15(PC5) ----> Sensor3 ADC_1 Channel_14(PC4) ----> Sensor4 ADC_1 Channel_9 (PB1) ----> Sensor5 ADC_1 Channel_8 (PB0) ----> Sensor6So above Channels available or not...?3) I have to get converted data from all channels .But how I can differentiate data of particular channels..?i.e when I have get data by statement below val= (int)ADC_GetConversionValue(ADC1); Then how I could Differentiate and Display Data of Particular channel..?4) Suppose I Have to print printf(''Channel11_data %d\n'',val); then printf(''Channel12_data %d\n'',val); . . . printf(''Channel_data8 %d\n'',val);For above thing to be done what are all the thing related to configuration and other I need to do..? plz guide me regarding that. #multi-channel-adc2013-11-11 1:48 AM
I think I've counted and enumerated them before, please check prior posts. You'll need the Data Manual for the part, and the User Manual for the board. You should be able to identify the free/usable pins.
For multiple channels you're supposed to use DMA, and an array that is a multiple of the sample list, you can then fish out your results in sequence from the array at TC and HT DMA interrupts. I've posted examples, and there should be others in the firmware libraries.2013-11-11 2:30 AM
''For multiple channels you're supposed to use DMA''
Why it is so..?
actually I not aware about programming uisng DMA
So will plz explain me why we can't use Interrupts for same and why u suggested DMA ..?
Will u please mentioned link regarding what u have mentioned ..?if possible then it will be very helpful for me. Because I have searched lot related to mentioned problem but i was not able to get specific post.Thanks a lot again for your valuable Responce.2013-11-11 4:41 AM
The primary reasons would be ones of speed and practicality. At 1Msps you're not going to be able to use interrupts to service the ADC, and the ADC does not provide an index. DMA puts them in an ordered array, the TC interrupt is the equivalent to a group EOC signal.
''13.8 Data management13.8.1 Using the DMA
Since converted regular channel values are stored into a unique data register, it is useful to use DMA for conversion of more than one regular channel. This avoids the loss of the data already stored in the ADC_DR register.
When the DMA mode is enabled (DMA bit set to 1 in the ADC_CR2 register), after each conversion of a regular channel, a DMA request is generated. This allows the transfer of the converted data from the ADC_DR register to the destination location selected by the
software.''
2013-11-12 10:43 PM
Once again Thanks clive1 for your valueable and Helpful responce.
I want to ask few things after this as follows1) I am using Two channel of ADC1 in continous mode and I want to print data continuously and at a time from both channels ..so how i can do it..?
e.g I have decalred
uint32_t ADC1_convertedValue[2];
then....
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADC1ConvertedValue;
.
.
.
...main function...
while(1)
{
val_ADC1_channel11 = ADC1ConvertedValue[0];
val_ADC1_channel12 = ADC1ConvertedValue[1];
printf(''Channel11_data %d\n'',val_ADC1_channel11);
printf(''Channel12_data %d\n'',val_ADC1_channel12);
}
..................
I want output of two statements as follows
Note : all values as randum and assumed by Myself Channel11_data 2049 Channel12_data 2016 Channel11_data 1826 Channel12_data 1650 Channel11_data 2144 Channel12_data 1866 . . .and so on....I think it may possible.I want to just confirm from you that it is so or not...?
2013-11-12 11:18 PM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/3%20channels%20on%20ADC1%20and%20DMA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=268]This thread about 7/8 th down