2018-05-29 09:24 PM
Hello ST engineers,
I have some questions about ADC of MCU STM32F302RC, please help to answer.
In our application, operating voltage of MCU is 3.3V (VDD=VDDA=3.3V). In firmware, we want to use VREFINT of ADC to calculate the VDDA to detect it.
According to the reference manual
, section 15.3.32 (Monitoring the internal voltage reference) at page 353/1080 described how to calculate VDDA with VREFINT. Here is the formula,Under normal operation, there is no problem. The calculated value of VDDA is right, and the value is about 3.29V which is almost equal to the actual power supply voltage.
But as long as the input voltage of PA0 (TTa, this port is used as ADC function, channel is ADC1_IN1) is subjected to a voltage greater than 3.65V, such as 3.75V, the calculated value of VDDA will be abnormal and become to about 1.22V. My question are,
1), why this phenomena happen?
2), as long as any channel of ADC is subjected to a higher voltage (greater than 3.65V), the calculated value of VDDA based on this formula will be abnormal, such as become to 1.22V?
3), when a normal GPIO (no ADC function) of the MCU is input a voltage greater than 3.65V, will this phenomena happen?
Thank you in advance!
2018-05-29 10:13 PM
Hello ST engineers,...
Not sure how many ST engineer are present here.
But as long as the input voltage of PA0 ... is subjected to a voltage greater than 3.65V, such as 3.75V, the calculated value of VDDA will be abnormal and become to about 1.22V.You are aware that you beyond specified limits, aren't you ? Proper functioning is not guaranteed.
I think protective diodes at the input pins begin to open up.
2018-05-29 11:03 PM
The protection diode is conducting and lifting your VDDA and so you will read a higher voltage,
Don't exceed the VDD on any pin. Otherwise your readings will be out.
Its like a rule, you can break the rule, but you will suffer the issues.
If you fix the problem, your issue will go away.
You can use lower voltage protection diodes outside the chip and feed with a resistor.
2018-05-30 12:55 AM
Hello Avatar,
Thanks for reminding, this is a forum, any engineer can read this problem and can answer.
Yes, because in the application, the condition of beyond specified limits can also happen, when the condition happened, the calculated value of VDDA become abnormal.
you are right, under this condition, proper function is not guaranteed. And what I want to know is that how the ADC will work when the input of ADC exceeds the upper limit? why it will affect the calculated value of VDDA? how does it affect the VDDA? etc.
here is the internal block diagram of IO port when ADC function is used. I don't know if the 3.75V is enough to make the protection diode work. but it is not important, because from the test result, as long as the ADC port is input a voltage greater than 3.66V, the calculated value of VDDA will become abnormal, regardless of whether the clamp diode working.
2018-05-30 01:14 AM
... any engineer can read this problem and can answer.
My point is - only the ST engineers know the internal circuits and parameters.
The others have to rely on official, published information, and guesses. Unfortunately, not many of ST's engineering staff is present here.
I used to protect my ADC inputs with a zener diode against excessive input voltages.
And you could spare a second AIN, and apply a fraction of VDD (VDD/2 ... VDD/10), to see if VDD is within bounds.
2018-05-30 01:33 AM
hello T J,
Thank you for reply.
1), first, I don't know if the diode can be conducted because of I don't know the Vf of the protection diode.
2), second, even the diode is conducting, why the VDDA is lifted? from the test result, we found the actual VDDA (observed by an oscilloscope and a multi-meter) has not changed at all (always is 3.3V) when the calculated value of the VDDA is abnormal (only is 1.22V).
3), use external diode with lower Vf (such as shottky diode), it is a good idea, but it is a protection method. in this topic, I still really want to know why this phenomena happened. in addition, for your suggestion of diode, we also tried before, and we found an interesting thing is that the lower Vf of diode you use, the higher leakage current of the diode. this also will cause some other issues, such as zero drift.
thanks!
2018-05-30 01:44 AM
hello AvaTar,
OK, I see.
use a zener diode (3.0V) is also the method what we adopted to solve this problem finally. thank you for your suggestion.
as long as the ADC input voltage is less than 3.66V (according to our test results), the calculated value of VDDA is correct, that is 3.3V.
2018-05-30 01:58 AM
the VDDA rail inside the processor must be affected, anyhow you can see the result.
Stop the high voltage before it gets to the chip. <- this is your work, don't put water in the fuel tank, its a rule too.
I use the ESD protection diodes, 2 diodes in one, and works for any pin. Something like this one.;
normally you would use a resistor, maybe 100R before the diodes to protect the high current into the new diodes.
2018-05-30 02:23 AM
hello T J,
yes, protection function should be always kept in mind when do designing.
our test circuit is very simple, just use a resistor divider (30K and 10K, made a ratio 1/4) to convert the external input voltage 0-10V to 0-2.5V as the ADC input. so there is 10K resistor between ADC port and GND. if you use the diode with high leakage current, the 10k will generate about several hundreds mV which will be input to ADC even there is no external analog voltage is supplied. such as the diode you suggest, the leakage current can up to 30uA under high temperature, and this Ir times by 10K will get 300mV, this is the zero drift what I said before and it should be avoided. (this is also the interesting thing (mentioned in the last reply to you) we found during experiment)
but, if use OPA circuit to replace the resistor divider at the ADC port, the Ir of the clamp diode does not need to be considered, at this time, the smaller Vf, the better.
thank you.