2024-11-27 7:14 AM
I’m encountering an issue with my STM32H755 application after moving the flash memory to accommodate SBSFU. The Reset_Handler address in the vector table is misaligned by one flash bank. Here are the details:
Background:
Problem: After moving my application to start at 0x08020400 to make room for SBSFU, the Reset_Handler address in the vector table is incorrect. The address is off by 0x203FF.
Linker Script: Here is the relevant part of my linker script:
MEMORY { FLASH (rx) : ORIGIN = 0x08020400, LENGTH = 896K RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 128K // Other memory regions } SECTIONS { .isr_vector : { . = ALIGN(8); KEEP(*(.isr_vector)) FILL(0); . = ORIGIN(FLASH) + LENGTH(FLASH) - 1; BYTE(0) . = ALIGN(8); } > FLASH .text : { . = ALIGN(4); *(.text) *(.text*) *(.glue_7) *(.glue_7t) *(.eh_frame) KEEP(*(.init)) KEEP(*(.fini)) . = ALIGN(4); _etext = .; } > FLASH // Other sections }
Startup Code: Here is the relevant part of my startup assembly file:
.section .isr_vector, "a", %progbits .type g_pfnVectors, %object .size g_pfnVectors, .-g_pfnVectors g_pfnVectors: .word _estack .word Reset_Handler .word NMI_Handler .word HardFault_Handler // Other exception vectors .thumb_func .type Reset_Handler, %function Reset_Handler: // Reset handler code b .
Vector Table Output: Here are the first 10 entries of the vector table:
0x08020400: 0x24020000 0x08020404: 0x080656E5 0x08020408: 0x08064549 0x0802040C: 0x0806454F 0x08020410: 0x08064555 0x08020414: 0x0806455B 0x08020418: 0x08064561 0x0802041C: 0x00000000 0x08020420: 0x00000000 0x08020424: 0x00000000
What I’ve Tried:
Question: Why is the Reset_Handler address in the vector table misaligned by one flash bank, and how can I fix this issue?
Solved! Go to Solution.
2024-11-27 9:32 AM
Resolved.
The SBSFU postbuild script that generates the .sfb firmware requires both the elf and bin files. I had not updated one of these after updating the flash address.
2024-11-27 9:32 AM
Resolved.
The SBSFU postbuild script that generates the .sfb firmware requires both the elf and bin files. I had not updated one of these after updating the flash address.