2024-11-05 11:33 PM
Hi all,
I failed to run Nucleo-G431RB board using Simulink "Monitor & Tune" mode via Simulink XCP protocol.
I've got the error message at Simulink,
"Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT command"
There has been no problem for Simulink "Build, Deploy & Start".
I followed an example from the link below.
https://www.mathworks.com/help/ecoder/stmicroelectronicsstm32f4discovery/ug/STM32F4XX-ADC-example.html
I've already changed Simulink model configuration to run Nucleo-G431RB LPUART.
- Hardware board = STM32G4xx Based
- Hardware board settings> Build options> Create> Select hardware = NUCLEO-G431RB
- Connectivity > USART/UART = LPUART1
- Connectivity > Serial port = COM1 (same port for STMicroelectronics STLink Virtual COM Port)
MATLAB related version:
- MATLAB 2023a
- Embedded Coder Support Package for ARM Cortex-M Processors V23.1.0
- Embedded Coder Support Package for STMicroelectronics STM32 Processors V23.1.3
STM32 related version:
- STM32CubeMX V.6.4.0
- STM32Cube_FW_G4_V1.5.1
I've read the similar post below, but couldn't figure out what was the problem.
https://community.st.com/t5/stm32-mcus-products/nucleo-g491re-communication-error-with-matlab-simulink-xcp/td-p/82065
Thank you in advance!
2024-11-05 11:39 PM
2024-11-05 11:40 PM
Hello @JellyFish and welcome to the ST Community.
For support on MATLAB/Simunlink, i suggest you to use the MATLAB Community https://www.mathworks.com/matlabcentral/content/communities.html.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.