cancel
Showing results for 
Search instead for 
Did you mean: 

Matlab Embedded Coder Build Error

shailjoshi007
Associate
Posted on December 26, 2015 at 22:30

While trying to build a simple LED simulink model using embedded coder I get the following error in last few lines of diagnosis report:

''C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/src/cmsis_rtos_init.c''

In file included from C:/MATLAB/SupportPackages/R2015a/STM32F4-Discovery_FW_V1.1.0/Libraries/CMSIS/ST/STM32F4xx/Include/stm32f4xx.h:245:0, 

                 from :0: 

C:/MATLAB/CMSIS-SP-00300-r4p5-00rel0/CMSIS/Include/core_cm4.h:151:0: warning: ''__FPU_USED'' redefined [enabled by default] 

       #define __FPU_USED       1U 

 ^ 

:0:0: note: this is the location of the previous definition

In file included from C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/src/cmsis_rtos_init.c:8:0: 

C:/MATLAB/SupportPackages/R2015a/armcortexm/toolbox/target/supportpackages/arm_cortex_m/cmsis_rtos_rtx/include/mw_cmsis_rtos.h:6:22: fatal error: cmsis_os.h: No such file or directory 

 #include ''cmsis_os.h'' 

                      ^ 

compilation terminated. 

gmake: *** [cmsis_rtos_init.o] Error 1

C:\Users\Shail\Documents\MATLAB\stm32f4discovery_gettingstarted_ert_rtw>echo The make command returned an error of 2  

The make command returned an error of 2 

 

C:\Users\Shail\Documents\MATLAB\stm32f4discovery_gettingstarted_ert_rtw>An_error_occurred_during_the_call_to_make 

'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command, 

operable program or batch file.

Please help me with this
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
shailjoshi007
Associate
Posted on December 27, 2015 at 18:27

Solved it. Had installed the latest version of CMSIS instead of CMSIS 4.2 which is recommended.