2013-11-15 5:06 AM
Hi all,
I'm working with STM32F3DISCOVERY.I'm trying to map the system clk on a GPIO to view it with an oscilloscope.In the following datasheethttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00058181.pdf
on page 39 I've found the signal SWCLK-JTCK that should be the system clock, but I didn't find any information on this signal. Do you know this signal?Thanks and regards #stm32f3discovery #swclk-jtck2013-11-15 6:31 AM
No that's a debugger clock.
To get system clocks, or fractions thereof, you need to look at MCO pins.2013-11-18 5:03 AM
Thank you Clive very much.
BTW can you tell me where the purpose ofSWCLK-JTCK
is indicated?Thanks and regards,2013-11-18 7:05 AM
Like I said it's part of the debug interface, combining with SWDIO to provide a clock/data channel for the SWD interface, or part of a higher pin count JTAG interface.
It's use is optional, if you don't use the debugger they can be GPIO or other AF2013-11-18 11:28 PM