2017-11-02 6:29 AM
Hi all,
i'm trying to customize html files that are hosted in a webserver running on my st32 nucleo f676zi with lwIP library.
The big issue is that i can't understand the correct usage of makefsdata script.
Actually, on a macbook, i call ./makefsdata and it works fine with html files, it generates a fsdata.c based on the folder on witch i have my html files.
But when i insert some .shtml files (SSI) the browser show me the pure html code without parsing it.
I think the problem should be on makefsdata script because with the original fsdata it works fine also with shtml files!
I found a .exe makefsdata here (
) but when it's running on windows 10 it crashes due to the missing of MSVCR100D.dll library that i'm not able to fix.Thanks in advance for the help.
2017-11-06 12:35 AM
Any suggestions? Thanks
2018-06-09 9:21 AM
>But when i insert some .shtml files (SSI) the browser show me the pure html code without parsing it.
edit the perl script and add the mime type for shtml