2021-12-23 2:35 AM
What is the difference between LPUART and UART?.
As far as i read there is no difference to use LPUART and normal one(except power consumption ofc). If I change my UART channel to LPUART, will be any difference? Will be the LP ones DMA usage differ from the normal one?
Any help will be appreaciated.
2021-12-23 3:31 AM
LPUART can work in deeper sleep modes and be used to wake up the CPU.
2021-12-23 7:06 AM
Please include your chip number in your post. Normal functions should be the same between the two, assuming the DMA connection exists.
2021-12-23 8:03 AM
For H7 series