cancel
Showing results for 
Search instead for 
Did you mean: 

Low layer examples

Curt Black
Associate II
Posted on September 22, 2017 at 17:46

Sometime between 1.6.0 and 1.9.0 the STM32CubeL4 package removed all of the examples_ll.

Is this intended, and where can I find the examples_ll now?

thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee
Posted on September 22, 2017 at 18:42

Hi,

You can find the Examples_LL under these paths:

STM32Cube_FW_L4_V1.9.0\Projects\STM32L476RG-Nucleo\Examples_LL

STM32Cube_FW_L4_V1.9.0\Projects\STM32L496G-Discovery\Examples_LL

STM32Cube_FW_L4_V1.9.0\Projects\STM32L496ZG-Nucleo\Examples_LL

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee
Posted on September 22, 2017 at 18:42

Hi,

You can find the Examples_LL under these paths:

STM32Cube_FW_L4_V1.9.0\Projects\STM32L476RG-Nucleo\Examples_LL

STM32Cube_FW_L4_V1.9.0\Projects\STM32L496G-Discovery\Examples_LL

STM32Cube_FW_L4_V1.9.0\Projects\STM32L496ZG-Nucleo\Examples_LL

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Curt Black
Associate II
Posted on September 22, 2017 at 18:56

The version I had downloaded did not have the Examples_LL directory.  There must have been a version where they were removed, then put back in.  (1.6.0 had them, 1.7.0 does not, 1.9.0 does have them)

I re-downloaded 1.9.0 and see they are back in.

thanks