cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 USBD receive

Dilbert K
Senior
Posted on September 22, 2017 at 15:45

I am currently using the 'STM32CubeFunctionPack_MOTENV1_V3.0.0' for SensorTile platform.

I does support the USBD_cdc function in sending data to PC (Print) but missing the receive code.

Since there is a ST BLE on board, I would like to connect with the 'BlueNRG GUI' tools which I can perform firmware update through USB for ST-BLE.

1. Where I could find the example code for USBD receive for STM32L4 ?

2. Is 'BlueNRG DK 2.0.2\Projects\Projects_Cube\BlueNRG_Stack_IFR_Updater' be the right package to start ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on September 22, 2017 at 18:57

Hi,

Have a look to the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubel4.html

firmware package to find the USB device example.

You have the

https://community.st.com/0D50X00009XkffXSAR

Bluetooth Low Energy software expansion for STM32Cube, you can start with thesample applications in Projects\Multi\Applications and followthe instructions provides in thereadme.txt file to run the example.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen