2008-09-01 8:37 PM
long long int division
2011-05-17 3:43 AM
Hi,
I have a problem in compiling in gcc long long int data type. I have linker error when I declare long long int as global variable and want to divide by another long long int variable. example that generate error: long long int a=1; long long int b=1; long long int c=1; void Fun1(void){ //Fun1 is called form another file a=1; } void Fun2(void){ a=b/c; } example that not generate error: long long int a=1; long long int b=1; long long int c=1; void Fun1(void){ a=1; } void Fun2(void){ Fun1(); a=b/c; } Can somebodey explain this? Error: Running : LD \''C:\Program Files\Raisonance\Ride\arm-gcc\bin\arm-none-eabi-gcc.exe'' -mcpu=cortex-m3 -mthumb -Wl,-T -Xlinker ''C:\Documents and Settings\jarek\Pulpit\Projekty\STM\GLCD\KS0108\4\FWLib\project\RIDE\STM3210B-EVAL\Project.elf.ld'' -u _start -Wl,-static -Wl,--gc-sections -nostartfiles -Wl,-Map -Xlinker ''C:\Documents and Settings\jarek\Pulpit\Projekty\STM\GLCD\KS0108\4\FWLib\project\RIDE\lst\Project.map'' c:/program files/raisonance/ride/arm-gcc/bin/../lib/gcc/arm-none-eabi/4.2.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-abort.o): In function `abort': abort.c.text+0x8): undefined reference to `_exit' c:/program files/raisonance/ride/arm-gcc/bin/../lib/gcc/arm-none-eabi/4.2.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-signalr.o): In function `_getpid_r': signalr.c.text+0x2): undefined reference to `_getpid' c:/program files/raisonance/ride/arm-gcc/bin/../lib/gcc/arm-none-eabi/4.2.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-signalr.o): In function `_kill_r': signalr.c.text+0x16): undefined reference to `_kill' c:/program files/raisonance/ride/arm-gcc/bin/../lib/gcc/arm-none-eabi/4.2.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-sbrkr.o): In function `_sbrk_r': sbrkr.c.text+0xc): undefined reference to `_sbrk' collect2: ld returned 1 exit status Build failed2011-05-17 3:43 AM
try to link with libgcc (-lgcc).
2011-05-17 3:43 AM
Hasn't this been answered on the Raisonance forum?
http://www.raisonance.com/Forum/punbb/viewtopic.php?pid=8718#p8718
If you're going to post the same question on different forums, you need to make sure that you keep every one updated. At least provide a link between the two!2011-05-17 3:43 AM
Quote:
On 02-09-2008 at 07:32, Anonymous wrote: Hasn't this been answered on the Raisonance forum?http://www.raisonance.com/Forum/punbb/viewtopic.php?pid=8718#p8718
If you're going to post the same question on different forums, you need to make sure that you keep every one updated. At least provide a link between the two! Hi, Thanks for the answer. Indeed the problem was solved on RIDE forum. They fix this problem in the Ride7 version 7.10.0000 and RKitARM version 1.10.0000. I am sorry for not update this forum :(