2023-12-18 1:00 AM
How in the world of programming is this possible? I got enough other problems to fix already.
It worked flawless before!
ld.exe: G431RBT6_Bootloader.elf section `.text' will not fit in region `FLASH'
ld.exe: section .applicationBlock LMA [000000000801f800,000000000801fa7b] overlaps section .text LMA [00000000080001e0,0000000008026e33]
ld.exe: region `FLASH' overflowed by 4294965884 bytes
Solved! Go to Solution.
2023-12-18 8:33 AM
Found the problem: i not just had a big object, i included whole libraries! I made my own lib which will run on STM32 and windows. It overflowed by over 4GB !
2023-12-18 1:41 AM
Hello @Tobe
4294965884 bytes is an enormous overflow of data
Look at the build analyzer or the map file for the build configuration that creates the elf file. It will show you what's consuming data.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-18 2:14 AM - edited 2023-12-18 2:14 AM
The build analyser shows nothing at all.
Here is the overview of the mapfile: (Highest number is like 0xXXXXX and 0xffffffffffffffff at *default* - "* ... *" means i left out text)
Discarded input sections
.text 0x0000000000000000 0x0
* ... (many 0x0000)*
Memory ConfigurationName Origin Length Attributes
RAM 0x0000000020000000 0x0000000000008000 xrw
FLASH 0x0000000008000000 0x0000000000020000 xr
*default* 0x0000000000000000 0xffffffffffffffff.isr_vector 0x0000000008000000 0x1d8
* ... *
0x000000000802b7c8 _sidata = LOADADDR (.data).data 0x0000000020000000 0x2d4 load address 0x000000000802b7c8
* ... *
0x00000000200022a0 . = ALIGN (0x8)/DISCARD/
libc.a(*)
libm.a(*)
libgcc.a(*).ARM.attributes
0x0000000000000000 0x30
* ... *
.ARM.attributes
0x0000000000002f84 0x1e * ... *none-eabi/10.3.1/thumb/v7e-m+fp/hard/crtn.o
OUTPUT(G431RBT6_Bootloader.elf elf32-littlearm)
LOAD linker stubs
LOAD * ... *../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc.a
LOAD * ... */.././../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libm.a
LOAD * ... *ib/gcc/arm-none-eabi/10.3.1/thumb/v7e-m+fp/hard\libgcc.a.debug_info 0x0000000000000000 0x15bd6
* ... *
2023-12-18 5:26 AM
It tells you the issue:
> ld.exe: section .applicationBlock LMA [000000000801f800,000000000801fa7b] overlaps section .text LMA [00000000080001e0,0000000008026e33]
You've allocated a large array or object that doesn't fit within the available memory. This would be done in your code, not the linker script.
2023-12-18 8:33 AM
Found the problem: i not just had a big object, i included whole libraries! I made my own lib which will run on STM32 and windows. It overflowed by over 4GB !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.