lin software on STM32F103 - Detecting stop bit errors
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-04 7:44 AM
I develop an own LIN slave node software stack for the STM32F103RB. This stack has to pass all tests from the LIN Conformance Test (according to ISO 17987-6). This test is a customer requirement.
Actually the software and/or the hardware could not detect error in the stop bits. (See test case PT-CT 38).
Is there a solution to detect a stop bit error during receiving or transmitting a data byte?
I could not find such a flag in the reference manual (RM0008).
Is there an undocumented feature to solve this problem?
- Labels:
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-18 3:19 AM
Hello @fehrlest ,
Please note that STM32 devices are general purpose MCUs not dedicated for automotive usage.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.