Question
Let the LED flash 3 times without using a blocking code
The point is that when you press a button, an LED should flash three times.
If you press the button again while it is flashing, the LED must flash 3 times again.
The whole thing should be implemented without blocking code.
I could could use a loop to make the LED blink 3x, but then I would have implicit blocking code in there again.
How can I implement this without blocking code?