Skip to main content
HTD
Senior II
May 26, 2023
Question

Launching the application doesn't work when "Build (if required) before launching" option is not checked.

  • May 26, 2023
  • 0 replies
  • 577 views

It doesn't work even when I manually do the build just before launching.

It doesn't work properly when checked either, because the build process is repeated each time although it's completely redundant, since the executable file is built and there are no unsaved changes to the code.

This topic has been closed for replies.