2025-08-17 8:47 PM - last edited on 2025-08-18 1:13 AM by Amel NASRI
Hi everyone,
I couldn't find the application note on STM32WB0 MCU hardware development. Can I refer to AN5290 which is for STM32WB instead of the STM32WB0. If so, is there anything I would need to pay attention to for the STM32WB0 series? Or should I reference from the NUCLEO-WB07CC's schematics instead?
Thank you for your time and help!
Solved! Go to Solution.
2025-08-18 12:02 AM
Hello @JTurn.2
The AN5290 is applicable only for the STM32WB series. For the STM32WB0, you can use the AN5129, the AN5526 and the design of the STM32WB0 Nucleo boards (NUCLEO-WB05KZ, the NUCLEO-WB07CC, and the NUCLEO-WB09KE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-18 12:02 AM
Hello @JTurn.2
The AN5290 is applicable only for the STM32WB series. For the STM32WB0, you can use the AN5129, the AN5526 and the design of the STM32WB0 Nucleo boards (NUCLEO-WB05KZ, the NUCLEO-WB07CC, and the NUCLEO-WB09KE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.