2012-04-05 4:03 AM
salut,
svp jr veux interfacer une clavier 4*4 avec un stm32 par les GPIO.... comment!!svp !!! NB : je met les 4 premier pins en 1 GPIO_SetBits(GPIOA,GPIO_Pin_0); GPIO_SetBits(GPIOA,GPIO_Pin_1); GPIO_SetBits(GPIOA,GPIO_Pin_2); GPIO_SetBits(GPIOA,GPIO_Pin_3);et j'esaye de faire le test sur les autres 4 pins !!!
#4x4-keypad2013-06-12 7:18 AM
And thus the indirect reference to a specific document with a diagram, and specific comment that PA4..7 have 100K pull-ups.
Seems a bit high to me. Keypads are usually a bit distant from the chip, so, let's assume 100pF stray capacitance giving a risetime of 100p * 100k ~ 10uS which, with fast code can be problematic.2013-06-13 12:40 AM
Well switches often bounce and human fingers aren't all that fast either. I don't see a problem with the pull up value.
You might have pointed out that some switches need a minimum ''wetting'' current. Depends on the switch and the application. Outside the scope of this forum really.