2023-06-13 1:47 AM
BLE_HearRateFreeRTOS example: latest .
; *************************************************************
; *** Scatter-Loading Description File generated by uVision ***
; *************************************************************
LR_IROM1 0x08000000 0x00080000 { ; load region size_region
ER_IROM1 0x08000000 0x00080000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x20000008 0x2FFF8 { ; RW data
.ANY (+RW +ZI)
}
RW_RAM_SHARED1 0x20030000 0x28 { ; RW data
*(MAPPING_TABLE)
}
RW_RAM_SHARED2 0x20030028 0x27D8 { ; RW data
*(MB_MEM1)
*(MB_MEM2)
.ANY (+RW +ZI)
}
}
How do I proceed?
2024-01-12 5:22 AM
I have the same but a little different problem:
BV_FULLBAND\Exe\Dory.axf: Error: L6244E: Exec region RW_IRAM1 address (0x20000004) not aligned on a 16 byte boundary.
I downloaded the STM32WB5MM sample project and compiled it in Keil µVision5. But this Error happens. I don't know how to handle it.
Do you have a solution since the problem happens or does anyone have the same problem but know how to solve it?
2024-01-12 7:00 AM
Perhaps just follow the direction and align the base address?
ie 0x20000010 and not 0x20000004
2024-01-12 7:01 AM
Likely a V6 compiler/link ABI issue
RW_IRAM1 0x20000040 0x2FFC0 { ; RW data, 64-byte alignment required