Jumping to Application
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-13 7:53 AM
Hi, I'm quite new with the ARM and STM32 world.
I'm developing an application wich has to load a bootloader and, at a certain point, jump to the main application. I'm using the STM32F4-Disco. The bootload is quite complex, using FreeRTOS and STemWin, comunicating to an external device with USART periph. Using a USB OTG drive which han an image.bin file on it (which is the main app code), I load it to a flash memory sector that for me is APPLICATION_ADDRESS (uint32_t)0x08080000 and then press a button on the touch-LCD for jumping to the loaded code. The jumping function is: cmd_Jump_To_Application(APPLICATION_ADDRESS) void cmd_Jump_To_Application(uint32_t start_Address) { USART_DeInit(USART2); USART_DeInit(USART1); RCC_APB2PeriphResetCmd(RCC_APB2Periph_USART1, ENABLE); RCC_APB2PeriphResetCmd(RCC_APB2Periph_USART1, DISABLE); RCC_APB1PeriphResetCmd(RCC_APB1Periph_USART2, ENABLE); RCC_APB1PeriphResetCmd(RCC_APB1Periph_USART2, DISABLE); RCC_DeInit(); __disable_irq(); uint32_t addressToJump = *(__IO uint32_t*) (start_Address + 4); pFunction Jump_To_Application = (pFunction) addressToJump; /* Initialize application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) start_Address); /* Call Reset Handler */ Jump_To_Application(); } Assuming that the downloading part to flash memory is right (I ported from the FW_Upgrade example, and debugging I can see what I expect in the application sector), there is something wrong. When I press the jump button I get a white screen and everything freezing and I can't start the main application. I'm missing something for sure, maybe about stack or some other vector adress\init, but I can't understand what. Some suggestions? Thanks!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 2:26 AM
Any help\suggestion? Thank you..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 2:42 AM
I could have swan I replied to this already! Must be the damn forum not accepting my replies again.
''After my main app launches, I get stucked in the USBH_OTG_ISR_Handler I think that this is because I don' DeInit the USB properly before the jump! I wrote a function USBH_Stop(&USB_OTG_Core,&USB_Host)'' I think the problem is the USB stop that you are doing. Instead try a USB soft Disconnect : void USB_SoftDisconnect( void ) { // set bit SDIS in OTG_FS_DCTL reg USB_OTG_dev.regs.DREGS->DCTL |= 0x02; }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 3:25 AM
Ahah, no problem! You are too kind!
Did you mean something like this? void USB_SoftDisconnect( USB_OTG_CORE_HANDLE *pdev ) { // set bit SDIS in OTG_FS_DCTL reg pdev->regs.DREGS->DCTL |= 0x02; } USB_SoftDisconnect( &USB_OTG_Core); I tried! Doing so, I get an hard falut starting my app, instead of going into the otg_handler. Not sure if better or worse! (I think worse)- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 4:27 AM
''I tried! Doing so, I get an hard falut starting my app, instead of going into the otg_handler.
Not sure if better or worse! (I think worse)'' It is better I think. Before, your bootloader was stuck due to USB IRQ. Now, your bootloader has started the application but you get a HardFault in Application. Debug your application. Find out why you get hard fault. (See if SysTick IRQ happens before it is set up - this happened to me).- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 8:32 AM
Actually it was stuck in the USB Handler, but already in the app, not in the bootloader!
Anyway I finally made it! The problem was related to the interrupts. __disable_irq(); suspend all interrups but does not act on the registers, so as soon as something in the App sets an interrupt, everything start acting random! I solved it writing this function and calling it just before the jump! void USB_Interface_DeInit(void){ RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE); RCC_AHB1PeriphResetCmd( RCC_AHB1Periph_OTG_HS, DISABLE); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, DISABLE); nvicStructure.NVIC_IRQChannel = OTG_HS_IRQn; nvicStructure.NVIC_IRQChannelPreemptionPriority = 15; nvicStructure.NVIC_IRQChannelSubPriority = 0; nvicStructure.NVIC_IRQChannelCmd = DISABLE; NVIC_Init(&nvicStructure); } Thank you again!!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-05-22 9:25 AM
I'm going to cross link this thread, as it picked up the SVC topic, and had similar issue with disabling interrupts vs servicing them in the application.
https://community.st.com/0D50X00009XkiGuSAJ
EDIT: Fixed DEAD LINK, Original from 22-May-2014
Up vote any posts that you find helpful, it shows what's working..

- « Previous
- Next »