cancel
Showing results for 
Search instead for 
Did you mean: 

JTAG Interface using a STM32F103

gmgunderground
Associate II
Posted on November 15, 2015 at 22:14

I want to develop a JTAG interface using STM32F103. One way is to use GPIO to drive/read the signals, another way is to use SPI, but unfortunately TMS signal is not present. Is there a way to use SPI and simulate a TMS sincronous with SPI clock ? Any other solution? Any suggestion is well come.

best regards

Gian

#stm32f103 #spi #jtag
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 15, 2015 at 22:56

The forum does not like mobile devices.

You'll have to decide if you can deal with the pins clashing or not. There are definitely a number of things to consider if you're doing boundary scan.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..