2023-07-24 03:28 PM - edited 2023-07-24 03:32 PM
Hello im creating one of my first stm32 boards and need some help ive watched many tutorials about decoupling capacitors and have referenced what i could from the datasheet could anyone confirm if this decoupling setup would work or if modifications are needed😀. I am using a usb-c connector for programming and power with an ams1117 3.3 volt regulator with the appropriate solid tantalum capacitors. For a little more info these are all smd 0603 capacitors and the component marked fb1 is a ferrite bead with a resitance of 120ohms at 100mhz.
Solved! Go to Solution.
2023-07-24 04:49 PM
> Wouldnt wiring the d+ and minus pins to the chip then using a 5,1k pulldown resistor to ground for the cc pins work?
Debugging requires a standalone debugger. They're cheap. I would recommend buying one, implementing the header on your board, and using that for debugging and programming. Here is one:
https://www.st.com/en/development-tools/stlink-v3minie.html
ST dev boards generally have an ST-LINK debugger built onto the dev board itself. It's a separate STM32 chip that sits between the target MCU and the USB.
2023-07-24 03:45 PM
Should work just fine. The ferrite bead isn't necessary if you aren't very concerned with analog performance.
> I am using a usb-c connector for programming
Through an STLINK-V3MINIE? Note that connecting USB directly to the chip itself won't allow for debugging.
For general reference, in case you haven't seen it:
2023-07-24 04:35 PM
Wouldnt wiring the d+ and minus pins to the chip then using a 5,1k pulldown resistor to ground for the cc pins work? then leaving the sbus1 and 2 pins unconnected should work? or not because i was looking of using usb c for programming without and extra board if there any ics that would work if my solution doesnt work and you knew of them could you give a link or a reference. thank you for your help anyways.
2023-07-24 04:49 PM
> Wouldnt wiring the d+ and minus pins to the chip then using a 5,1k pulldown resistor to ground for the cc pins work?
Debugging requires a standalone debugger. They're cheap. I would recommend buying one, implementing the header on your board, and using that for debugging and programming. Here is one:
https://www.st.com/en/development-tools/stlink-v3minie.html
ST dev boards generally have an ST-LINK debugger built onto the dev board itself. It's a separate STM32 chip that sits between the target MCU and the USB.
2023-07-24 06:18 PM
Unless my eyes are playing tricks, it looks like you have 12 VDD pins and 11 0.1u bypass caps. Probably best to make sure there is a cap on each VDD pin.
2023-07-24 06:25 PM
...and FWIW, tantalum is considered a 'conflict' material. I don't think I've see tantalum caps in a design for years. I cannot speak to the necessity of using tantalum, though. I can say that the LDOs I've used have generally stated that they can provide stable regulation with ceramics. Often, though, I'm only looking for a few 100mAs. Once we get to the range of 1A, generally we place a buck regulator (e.g. ACOT) for better efficiency and these, too, operate fine with ceramic caps.
2023-07-24 10:27 PM
Tantalum - wasn't that something last seen in the 90s? :D
Depending on what else is powered from these 3.3V, a switching regulator might be more appropriate than the LDO. Check power dissipation.
And I would also recommend putting the SW DEBUG pins on a header.
And take care of the boot pins, at least that you can access them in case you need to.
2023-07-24 10:48 PM
I think folks still use tantalum because datasheets, like this one, recommend it. I was curious about the part since I hadn't seen it placed. It's quite inexpensive. It also expects a large output capacitor to stabilize the output. Modern LDOs operate fine with 1u. This device recommends 22u.
At 1A, you're looking at (5-3.3)*1W dissipation, so roughly 2W. Shrug. It'll get warm. The DS makes it look like it can handle this configuration. If it is mounted over a large copper, it should survive.
2023-07-25 03:14 AM
I guess he will not need 1A, because for 1.7W you need a lot of thick copper or some other cooling.
Anyway, even for space reasons I would check what the max. current requirement is, then decide if a switching regulator makes sense - or even if a SOT23-5 LDO might be enough.
Interestingly, there are almost pin-compatible LDO / buck regulators in SOT23-5/6 out there, so for some designs I basically put the buck circuit on the board, but if an LDO was good enough, I just bridged the inductor:
2023-07-30 03:57 PM
Yep i saw it too just forgot to place one i guess😀