2019-10-29 8:48 AM
2019-10-29 8:57 AM
Haven't looked but should allow for HT/TC interrupts to curate a Ping-Pong buffer, unpack data directly into the inactive half, rather than copy buffers.
Perhaps look at newer lower power and more capable parts.
2019-10-29 1:29 PM
Double-buffering is only in the two-port DMAs, i.e. in 'F2/'F4/'F7/('H7).
Clive's advice sounds viable.
Another trick - at a cost of some timers and DMA channels - might perhaps be, not to feed DAC using DMA channel triggered by DAC itself, but to feed it from a DMA channel triggered by a suitably timed timer. Then, you could use two such channels and switch between them just by enabling/disabling timers and/or the DMA channels, when needed.
JW
PS. Please change your username to a normal nick.