2018-08-21 08:42 AM
The dev kit documentation states that the module runs on the 860-930 MHz range that, according to the transceiver doc, should be the band 1.
Does anyone know if it's possible to change the band to 2 or 3? Or there is any limitation for that?
Thank you in advance to the community!
2018-08-21 09:36 AM
All the source code is provided, you can adapt the frequencies/bands to support your specific application/use-case
2018-08-21 03:50 PM
Thank you Clive. So this means that data in the documentation is a bit misleading...