cancel
Showing results for 
Search instead for 
Did you mean: 

Is interbal RC Osc accurate enough for serial UART TS232 for STM32F103RB?

john1389
Associate II
Posted on July 22, 2016 at 22:31

Is it true that 2 to 3% accuracy is required? 

Nucleo F103 has no crystal. Nucleo F401 has 32kHz crystal
2 REPLIES 2
Posted on July 22, 2016 at 23:12

> Is it true that 2 to 3% accuracy is required? 

Yes.

JW

Posted on July 23, 2016 at 01:14

Both Nucleo boards can take an 8 MHz clock source from the ST-LINK chip which does have an HSE clock.

USARTs can tolerate a fair amount of clock error.

The LSI is not only likely to be off in frequency, but it also changes (poor stability). Can't say I've spent a lot of time looking at the HSI, but have got some boards wired to a GPS 1PPS source so could probably evaluate it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..