Skip to main content
john1389
Associate
July 22, 2016
Question

Crystal accuracy for USB

  • July 22, 2016
  • 1 reply
  • 844 views
Posted on July 22, 2016 at 22:58

What ppm accuracy is needed for STM32F103RB as full-speed (12Mbits/s) device?

Is RC HSI (a few percent error) not accurate enough for STM32F103RB as USB device?

For STM32F401RE, do host or OTG modes require higher accuracy than device mode? 

Does Device 'listen to and derive' clocking speed from Host/OTG and requires less accurate crystal?   

#usb-crystal-accuracy
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
July 22, 2016
Posted on July 22, 2016 at 23:11

> Is RC HSI (a few percent error) not accurate enough for STM32F103RB as USB device?

No. From USB2.0, 7.1.11:

 

The full-speed data rate is nominally 12.000 Mb/s. For full-speed only functions, the required data-rate when

 

transmitting (T FDRATE ) is 12.000 Mb/s  ± 0.25% (2,500 ppm).

 

 

JW