cancel
Showing results for 
Search instead for 
Did you mean: 

IrDA compliant library

shotaro
Associate II
Posted on May 09, 2012 at 00:56

One of the areas I'm looking at with the STM32 is being able to transfer files (or at least data) from an IrDA dongle from Windows to the STM32. However, as I understand it, the STM32 only implements the PHY layer using SIR, and it's missing the other two mandatory layers (IrLAP and IrMP), which I'm assuming is software based.

Is there any library out there that I could use for the STM32 that is IrDA compliant and/or can interface with Windows?

EDIT: Actually never mind. It took me a while to find out some folks make a raw IR to serial adapter, which would be even better in this case.

#irda
1 REPLY 1
ELai
Associate

could you please share what "raw IR to serial adapter" to use?

i need a short range (10cm) wireless communication