2024-09-08 09:24 AM - last edited on 2024-09-08 11:25 AM by Peter BENSCH
good morning. i have a problem regarding button and time interrruptions. for the button, i linked it to the mcu but i do not know if i have to put the input as gpio or wake up, moreover, i do not know how to use the IRQ GUI, i do not know how it works or the code to put in it. the samples examples are not made for my spc58ec and do not use the applications directly. for the time interruption i have the same problem. i want to use asimple led blinking like in the example below , the interruption would turn it into high or low.
best regards