cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt - running from ext flash

sudano
Associate
Posted on March 08, 2011 at 09:21

Interrupt - running from ext flash

1 REPLY 1
picguy2
Associate II
Posted on May 17, 2011 at 14:27

If I remember correctly the interrupt vector can not reside in external memory.  It's best in flash but internal RAM works.  External memory is S...L...O...W.  Whenever possible copy to internal RAM for execution.

A reasonable mindset is external memory = disk.  Not true but it gets you to think in terms of overlays.