2013-11-19 8:28 AM
I have a problem with my Interrupt priority....
My TIM3 is called every 5ms and have high priority and my TIM2 every 1ms have low priority and everytime my TIM2 is called. I want Interrupt TIM2 when TIM3 is active where is the problem ? void Config_Timer_TIM2(TIM_TimeBaseInitTypeDef *TIM_TimeBaseStructure, NVIC_InitTypeDef *NVIC_InitStructure) { RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Enable the Timer2 Interrupt */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure->NVIC_IRQChannel = TIM2_IRQn; // configure the Timer2 interrupts NVIC_InitStructure->NVIC_IRQChannelPreemptionPriority = 0x0F; // sets the priority group of the TIMER2 interrupts NVIC_InitStructure->NVIC_IRQChannelSubPriority = 0; // set the subpriority inside the group NVIC_InitStructure->NVIC_IRQChannelCmd = ENABLE; // TIMER2 interrupts are globally enabled NVIC_Init(NVIC_InitStructure); /* Configure Timer which is every 1 ms active*/ TIM_DeInit(TIM2); TIM_TimeBaseStructInit(TIM_TimeBaseStructure); /* Time base configuration */ TIM_TimeBaseStructure->TIM_Prescaler = 360 - 1; // 72 MHz / 360 = 200 khz TIM_TimeBaseStructure->TIM_Period = 200 - 1; // (1/200khz) * 200 = 1 ms; TIM_TimeBaseStructure->TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure->TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, TIM_TimeBaseStructure); //TIM_PrescalerConfig(TIM2, 360-1 , TIM_PSCReloadMode_Immediate); /* Enable TIM2 Update Interrupt */ TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); /* Enable TIM2 */ TIM_Cmd(TIM2,ENABLE); } void Config_Timer_TIM3(TIM_TimeBaseInitTypeDef *TIM_TimeBaseStructure, NVIC_InitTypeDef *NVIC_InitStructure) { RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* Enable the Timer3 Interrupt */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure->NVIC_IRQChannel = TIM3_IRQn; // configure the Timer2 interrupts NVIC_InitStructure->NVIC_IRQChannelPreemptionPriority = 0 ; // sets the priority group of the TIMER2 interrupts NVIC_InitStructure->NVIC_IRQChannelSubPriority = 0; // set the subpriority inside the group NVIC_InitStructure->NVIC_IRQChannelCmd = ENABLE; // TIMER3 interrupts are globally enabled NVIC_Init(NVIC_InitStructure); /* Configure Timer which is every 5 ms active*/ TIM_DeInit(TIM3); TIM_TimeBaseStructInit(TIM_TimeBaseStructure); /* Time base configuration */ TIM_TimeBaseStructure->TIM_Prescaler = 1800 - 1; // 72 MHz / 1800 = 40 khz TIM_TimeBaseStructure->TIM_Period = 200 - 1; // (1/400khz) * 200 = 5 ms; TIM_TimeBaseStructure->TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure->TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, TIM_TimeBaseStructure); /* Enable TIM2 Update Interrupt */ TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE); void TIM2_IRQHandler(void) { Display_Adc_Value(Line7,Black,Line3,Green,ADC1); Display_Adc_Value(Line8,Black,Line5,Blue,ADC2); TIM_ClearITPendingBit(TIM2, TIM_IT_Update); //Update Interrupt } void TIM3_IRQHandler(void) { UARTSend(''CV'', 1); // if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET) // { // // } TIM_ClearITPendingBit(TIM3, TIM_IT_Update); //Update Interrupt }2013-11-19 11:33 AM
remove the output calls from your ISRs (it is, generally a bad idea to call non-related output from ISRs) and just set/clesr a flag, then use the debug to see what happens.
Erik