2008-01-13 12:06 PM
Interfacing STM32 to multiple external ADCs
2011-05-17 3:21 AM
Hi
I'm pretty new with the STM32 and I'm wondering if one could interface the STM32 to an multiple external ADC, eg 4 x 24bit? The ADCs will be squirting serial data out. Instead of using FPGA to interleave the data, I was thinking of using the STM32 to do the job. Any advice or example is greatly appreciated.