2014-05-09 1:09 PM
Hello everybody.
I want to solve a read problem in a special hardware, the configuration of each pin is input:RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE, ENABLE);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;GPIO_Init(GPIOC, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_6 | GPIO_Pin_10;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_Init(GPIOC, &GPIO_InitStructure);there many pins work...my problem is in the next code (this is a function in my library):unsigned int ReadData(void){ unsigned char nop=eco;//eco=5, is a delay. unsigned int data = 0; unsigned char count=0; for(count=0; count<12; count++) { data <<= 1; GPIO_SetBits(GPIOC, GPIO_Pin_10); while(nop!=0){nop--;} nop=eco; GPIO_ResetBits(GPIOC, GPIO_Pin_10); while(nop!=0){nop--;} nop=eco; if (GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_8)); {data++;} } return(data);}when I read the value in data, only I read 0xFFF (12 bits) in all cases, but I see signals for example 0x34F or 0x584 many combinations and I saw a good synchronization with the clockusing a analyzer logic. maybe is the configuration of the inputs but I 'm not sure.thank you in advance. #input-configuration2014-05-09 1:20 PM
Make nop volatile
2014-05-09 1:37 PM
Thank you for your speed answer, but sorry, How is ''Make nop volatile''?
do I make it in the variables of the function ReadData? because the variable ''nop'' is only a delay but it isn't important, the most important value is Data but when I return this, the value is all ones (0xFFF).thank you so much.2014-05-09 1:51 PM
volatile unsigned char nop=eco;//eco=5, is a delay.
This way the compiler won't optimize it away. When does the data line come valid with respect to the pulse sent out? There are pipeline and synchronization delays with respect to reading bits back. Are you sure you are looking at the right bit, can you ever read the pin low?2014-05-09 2:29 PM
Thank you for the information about the volatile in the variable ''nop''.
mm.. I'm reading the registers 0x90 and 0xD0 on the XPT2046 and the communication protocol like this.http://www.sunrom.com/media/content/557/images/signals.gifSPI communication.When does the data line come valid with respect to the pulse sent out?A: is when I write the 0x90 and dthe 0xD0 in another stage of my code, but I look the shipping of the data and it's correct and have a good synchronization .Are you sure you are looking at the right bit, can you ever read the pin low?A:yes, I'm sure :\ the code emule the SPI through software for eliminate error of configurations or bugs. I looked different values between 0x010 and 0xFE0 and never is the maximun value(0xFFF) at least I never looked this (because the limitation of the hardware the resistive panel).there is a correct synchronization or so it seems.2014-05-09 2:29 PM
I changed the pin, the pin PC8 was changed by PA1 and I have the same result, I think the problem is the configuration when I use the instruction ''GPIO_ReadInputDataBit'' only read '1'.
:(2014-05-09 6:13 PM
Get rid of the semi-colon at the end of the 'if' line
if (GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_8)); // <-- DON'T PUT THAT SEMICOLON HERE
{data++;}