2018-02-28 2:35 AM
Hi,
I am using
STM32F446RETxNucleo board formy application. It was working fine till I added a new operations including asynchronous data exchange on UART5. Now
, sometimes during data exchange on the serial channel, the debbuger (the application is written in Truesudio, using HAL libraries) jumpes into thisInfinite_Loop:/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
* @param None
* @retval None
*/
.section .text.Default_Handler,'ax',%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
.
.
.
The comment of the loop says that there might be an 'unexpected interrupt', however inside the startup file (startup_stm32f446xx.s) I see all my interrupts and their 'weak descriptions'. I also controlled the code several times and it seems to be fine.
So, I have two questions: first, how can I discovert which interrupt caused this problem? then, do you have any advice to handle this problem?
I appreciate any hint on this matter! Thank you!
#infinite_loop #startup-file #uart-interrupt-stm32f42018-02-28 3:20 AM
Almost always a missing or misspelled IRQ Handler name.
You could have a build where you make them non-weak and see which ones the linker indicates are already defined. You could check the enabled peripherials for an active interrupt flags.
Check UART vs USART naming .
2018-02-28 3:20 AM
Wouldn't Truestudio have a call stack display in debugger mode, where you see what it came from ?
Otherwise, check the SCB registers for error flags.
But the UART interrupt would be the prime suspect.
2018-02-28 6:32 AM
Thank you for the reply!
First of all, as far as I know, stack display or analyzer of TrueStudio is not available on the free version that I am using.
Then, I don't think that it is the UART interrupt, because the problem does not happen with all the serial data exchanges. Usually, I can have several data exchanges before encountering the Infinit_Loop.
About the SCB, I looked in it, but, actually I do not really know what should I look for.
2018-02-28 6:40 AM
TrueStudio is now free of charge for all STM32 users. Meaning the previous Pro version now is free:
https://atollic.com/resources/download/windows/
Maybe some code would be useful do understand what's wrong.
2018-02-28 6:46 AM
Thank you Clive One,
Actually, the startup file is created automatically. I used CubeMX to start the project and everything is done using the standard procedures. Moreover, I confronted, manually and by using search feature of the editor, each interrupt implemented inside stm32f4xx_it with the contens of the startup file. They were all identical. However, I also need to check the interrupt flag that you mentioned!
2018-02-28 7:56 AM
Thank you! I've just installed it.
2018-02-28 7:59 AM
About the SCB, I looked in it, but, actually I do not really know what should I look for.
The linked document should give you some explanations:
http://www.keil.com/appnotes/files/apnt209.pdf
I don't use Cube, and don't comment on this kind of auto-generated code.
Perhaps you end up in the hardfault handler, either because of a stack overflow, or another, unhandled exception.
The SCB register flags will tell you.