2023-03-15 7:02 AM
"64 Kbytes located at address 0x0A03 0000 with hardware parity check (SRAM2). This memory is also mapped at address 0x2003 0000 offering a contiguous address space with the SRAM1"
2023-03-20 7:14 AM
Hi @sra ,
look at the memory map figure in the reference manual (chapter 2.3.2).
The same physical memory is accessed on different address ranges depending on the access type. Non-secure or non-secure callable for code, non-secure or secure if data.
If the TZ on your device is disabled or configured to have the SRAM2 non-secure, you should be able to access the SRAM2 at 0x2003 0000.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.