cancel
Showing results for 
Search instead for 
Did you mean: 

ICMP Ping Failure to Google After PPP Connection on STM32F407

Noushadalik
Associate III

Hi, 
https://community.st.com/t5/stm32-mcus-products/configuring-ppp-on-stm32f407disc-with-lte-modem-via-usart-using/m-p/728673#M262741 

This continues the previous thread discussing the PPPoS implementation for the STM32F407. I successfully established a PPP connection and obtained an IP address. However, my ICMP ping to Google did not receive a successful response. Please check the code snippet below for any necessary changes.


 

void PPPosClientThread() { osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); pppos_task_started = 1; osSemaphoreRelease(pppos_mutex); int gsmCmdIter = 0; int nfail = 0; printf("GSM: Starting Modem thread\r\n"); char* data = (char*) malloc(BUF_SIZE); char PPP_ApnATReq[sizeof(CONFIG_GSM_APN) + 24]; sprintf(PPP_ApnATReq, "AT+CGDCONT=1,\"IP\",\"%s\"\r\n", CONFIG_GSM_APN); cmd_APN.cmd = PPP_ApnATReq; cmd_APN.cmdSize = strlen(PPP_ApnATReq); //_disconnect(1); // Disconnect if connected // FOR testing osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); pppos_tx_count = 0; pppos_rx_count = 0; gsm_status = GSM_STATE_FIRSTINIT; osSemaphoreRelease(pppos_mutex); // GSM reset pin functionality required enableAllInitCmd(); while (1) { while (gsmCmdIter < GSM_InitCmdsSize) { if (GSM_Init[gsmCmdIter]->skip) { #if GSM_DEBUG infoCommand(GSM_Init[gsmCmdIter]->cmd, GSM_Init[gsmCmdIter]->cmdSize, "Skip command:"); #endif gsmCmdIter++; continue; } if (atCmd_waitResponse(GSM_Init[gsmCmdIter]->cmd, GSM_Init[gsmCmdIter]->cmdResponseOnOk, NULL, GSM_Init[gsmCmdIter]->cmdSize, GSM_Init[gsmCmdIter]->timeoutMs, NULL, 0) == 0) { // * No response or not as expected, start from first initialization command #if GSM_DEBUG printf("GSM: Wrong response, restarting...\r\n"); #endif nfail++; if (nfail > 20) goto exit; osDelay(3000); gsmCmdIter = 0; continue; } if (GSM_Init[gsmCmdIter]->delayMs > 0) osDelay(GSM_Init[gsmCmdIter]->delayMs); GSM_Init[gsmCmdIter]->skip = 1; if (GSM_Init[gsmCmdIter] == &cmd_Reg) GSM_Init[gsmCmdIter]->delayMs = 0; // Next command gsmCmdIter++; } #if GSM_DEBUG printf("GSM: GSM initialized.\r\n"); #endif osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); if(gsm_status == GSM_STATE_FIRSTINIT) { osSemaphoreRelease(pppos_mutex); // ** After first successful initialization create PPP control block ppp = pppos_create(&ppp_netif, ppp_output_callback, ppp_status_cb, NULL); if (ppp == NULL) { #if GSM_DEBUG printf("GSM: Error initializing PPPoS\r\n"); #endif break; // end task } } else osSemaphoreRelease(pppos_mutex); //ppp_set_default(ppp); netif_set_default(&ppp_netif); //ppp_set_auth(ppp, PPPAUTHTYPE_ANY, "", ""); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); gsm_status = GSM_STATE_IDLE; osSemaphoreRelease(pppos_mutex); ppp_connect(ppp,0); while(1) { // === Check if disconnect requested === osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); if (do_pppos_connect <= 0) { int end_task = do_pppos_connect; do_pppos_connect = 1; osSemaphoreRelease(pppos_mutex); #if GSM_DEBUG printf("\r\n"); printf("GSM: Disconnect requested.\r\n"); #endif ppp_close(ppp, 0); int gstat = 1; while (gsm_status != GSM_STATE_DISCONNECTED) { // Handle data received from GSM memset(data, 0, BUF_SIZE); int len = UART_Read(data, BUF_SIZE, 30); if (len > 0) { pppos_input_tcpip(ppp, (u8_t*)data, len); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); pppos_tx_count += len; osSemaphoreRelease(pppos_mutex); } osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); gstat = gsm_status; osSemaphoreRelease(pppos_mutex); } osDelay(1000); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); uint8_t rfoff = gsm_rfOff; osSemaphoreRelease(pppos_mutex); _disconnect(rfoff); // Disconnect GSM if still connected #if GSM_DEBUG printf("GSM: Disconnected.\r\n"); #endif gsmCmdIter = 0; enableAllInitCmd(); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); gsm_status = GSM_STATE_IDLE; do_pppos_connect = 0; osSemaphoreRelease(pppos_mutex); if (end_task < 0) goto exit; // === Wait for reconnect request === gstat = 0; while (gstat == 0) { osDelay(100); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); gstat = do_pppos_connect; osSemaphoreRelease(pppos_mutex); } #if GSM_DEBUG printf("\r\n"); printf("GSM: Reconnect requested.\r\n"); #endif break; } // === Check if disconnected === if (gsm_status == GSM_STATE_DISCONNECTED) { osSemaphoreRelease(pppos_mutex); #if GSM_DEBUG printf("\r\n"); printf("GSM: Disconnected, trying again...\r\n"); #endif ppp_close(ppp, 0); _disconnect(1); enableAllInitCmd(); gsmCmdIter = 0; gsm_status = GSM_STATE_IDLE; osDelay(10000); break; } else osSemaphoreRelease(pppos_mutex); // === Handle data received from GSM === memset(data, 0, BUF_SIZE); int len = UART_Read(data, BUF_SIZE, 50); if (len > 0) { //printf("RX: %d\r\n", len); //printf("data :%s\r\n",data); pppos_input_tcpip(ppp, (u8_t*)data, len); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); pppos_tx_count += len; osSemaphoreRelease(pppos_mutex); } } // Handle GSM modem responses & disconnects loop } // main task loop exit: if (data) free(data); // free data buffer if (ppp) ppp_free(ppp); osSemaphoreWait(pppos_mutex, PPPOSMUTEX_TIMEOUT); pppos_task_started = 0; gsm_status = GSM_STATE_FIRSTINIT; osSemaphoreRelease(pppos_mutex); #if GSM_DEBUG printf("GSM: PPPoS TASK TERMINATED\r\n"); #endif //osThreadTerminate(mythread); }
View more

 

Ping code snippet:

 

void start_ping_action() { //get gateway IP from global net interface ip_addr_t gw_addr = ppp_netif.ip_addr; uint8_t gw_ip_part_1 = ip4_addr1(&gw_addr); //check if DHCP already succeeded by checking against non 0 ip part int ret = 0; if(gw_ip_part_1 != 0) { ip_addr_t target_ping_ip; //select target: //gateway //target_ping_ip = gw_addr; //static IPs //IP_ADDR4(&target_ping_ip, 192,168,1,180); IP_ADDR4(&target_ping_ip, 216,58,213,195); //google.com //IP_ADDR4(&target_ping_ip, 8, 8, 8, 8); // Google's DNS printf("Starting to ping IP: %d.%d.%d.%d.\r\n", (int)ip4_addr1(&target_ping_ip), (int)ip4_addr2(&target_ping_ip), (int)ip4_addr3(&target_ping_ip), (int)ip4_addr4(&target_ping_ip)); if((ret = ping_ip(target_ping_ip)) != PING_ERR_OK) { printf("Error while sending ping: %d\r\n", ret); } } //every 4 seconds, start a new ping attempt sys_timeout(4000, start_ping_action, NULL); } void check_ping_result() { ping_result_t res; memset(&res, 0, sizeof(res)); int retcode = 0; if((retcode = ping_ip_result(&res)) == PING_ERR_OK) { if (res.result_code == PING_RES_ECHO_REPLY) { printf("Good ping from %s %u ms\r\n", ipaddr_ntoa(&res.response_ip), (unsigned) res.response_time_ms); } else { printf("Bad ping err %d\r\n", res.result_code); } } else { //printf("No ping result available yet: %d\n", retcode); } sys_timeout(100, check_ping_result, NULL); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */
View more

 



Output logs:

 

UART6 init done GSM: Starting Modem thread GSM: AT COMMAND: [AT..] GSM: AT RESPONSE: [..OK..] GSM: AT COMMAND: [ATD*99#..] GSM: AT RESPONSE: [..CONNECT 115200..] GSM: GSM initialized. GSM: ppp_status_cb: 0 GSM: status_cb: Connected GSM: ipaddr = 10.220.50.XXX GSM: gateway = 10.64.64.XX GSM: netmask = 255.255.255.255 GSM: LTE Init done Starting StartDefaultTask IP:10.220.50.142 Starting to ping IP: 216.58.213.XXX. Ping timed out Bad ping err 0 Starting to ping IP: 216.58.213.XXX. Ping timed out Bad ping err 0 Starting to ping IP: 216.58.213.XXX. Ping timed out Bad ping err 0 Starting to ping IP: 216.58.213.XXX.

 



1 ACCEPTED SOLUTION

Accepted Solutions

No updates... still the same advice.

View solution in original post

6 REPLIES 6
Pavel A.
Super User
Noushadalik
Associate III

Hello,
Any update today?

No updates... still the same advice.

Hi @Pavel A. 
Are you ST employee?

No I am not.

Noushadalik
Associate III

Hello,

I would greatly appreciate any assistance with the LTE modem PPPoS implementation for the STM32F407, as well as any related documents or information you could share.
Thank you!