2021-03-16 10:34 AM
Hi
I'm using IAR EW for ARM.
I would like to get a simple working project that is made for the STM32F767ZI processor, preferably running on a Nucleo-144 board.
The example should only make the initialisation of the processor. I'm making a Bootloader so I don't think I need much more. I'm just worried with putting the Processor clock working.
I'll be using FreeRTOS IP stack but for now I only need the processor starting.
In there any Wizard for IAR that creates a simple example project running on the Nucleo-144?
thanks
Solved! Go to Solution.
2021-03-16 11:03 AM
Like
STM32Cube_FW_F7_V1.16.0\Projects\STM32F767ZI-Nucleo\Templates\EWARM
2021-03-16 11:03 AM
Like
STM32Cube_FW_F7_V1.16.0\Projects\STM32F767ZI-Nucleo\Templates\EWARM