cancel
Showing results for 
Search instead for 
Did you mean: 

IAP - PC side

greg_t
Associate II
Posted on October 21, 2010 at 21:30

IAP - PC side

4 REPLIES 4
Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:12

One of the main reasons for using YMODEM (or XMODEM) is that just about every terminal program suports it.

So you can use any terminal program you like (provided it has YMODEM).

See:

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Hyperterminal%20is%20not%20the%20only%20terminal%20program

!!

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:12

the XMODEM and YMODEM specifications are available & free on the net, and it's not hard to write your own implementation.

http://www.lmgtfy.com/?q=xmodem+ymodem+protocol+specification

Most serial coms libraries will include X- and/or Y-MODEM...

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:12

I know - that is a really stupid, misleading, and unhelpfulthing that it says!

Sorry, the forum broke the link I posted earlier - try this one:

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/Hyperterminal is not the only terminal program!!&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&currentviews=260

lowpowermcu
Associate II
Posted on May 17, 2011 at 14:12

Hi Andrew,

I have discovered that in the available version in ST site, it is mentioned

''To use the IAP, the user must have a PC running HyperTerminal or other Terminal program that supports ymodem protocol. In this document the HyperTerminal is used.''

:-)

regards,

MCU Lüfter