2023-04-12 12:25 PM
I figured to increase the volume of the pcm data i just multiply it, because it is pretty much a sine wave sampled? I use this to increase the volume of the audio from the microphone connected to i2s and it works great. I do this when the audio is still 24 bit( 32bit frame) and later convert it to 16 bit as this is the required format for my android application. But when i receive 16 bit audio send from the android app to the stm32 and i multiply the 16 bit value by any number, there is a huge amount of noise. any idea why? (microphone uses i2s and dac uses sai in i2s mode) (and i convert the stereo to mono in my microphone function).
if(uart_to_audio_rd_ptr != uart_to_audio_wr_ptr){
for(int i =0; i < buffer_size/2; i+=2){
int16_t little_endian_value = ((int16_t)uart_to_audio_buffer[uart_to_audio_rd_ptr+i+1] << 8) | (int16_t)uart_to_audio_buffer[uart_to_audio_rd_ptr+i];
int16_t big_endian = (int16_t)__REV16(little_endian_value);
int32_t out = big_endian*1;
if(out>32767) out = 32767;
else if(out<-32768) out = -32768;
int16_t out2 = out & 0xFFFF;
audio_out[i] =(out2>> 8) & 0xFF;
audio_out[i+1] = out2 & 0xFF;
}
uart_to_audio_rd_ptr += buffer_size/2;
if(uart_to_audio_rd_ptr >= main_buffer_size) uart_to_audio_rd_ptr = 0;
}
}void HAL_I2S_RxHalfCpltCallback (I2S_HandleTypeDef *hi2s){
for (uint16_t i = 0; i < buffer_size/4; i++) {
int lSample = (int) (audio_in[4*i+2]<<16)|audio_in[4*i+2+1];
lSample = lSample*10;
if(lSample>2147418112)
{
lSample = 2147418112;
}
else if(lSample<-2147483648)
{
lSample = -2147483648;
}
int16_t top16 = (lSample >> 16) & 0xFFFF;
int16_t little_endian_value = (int16_t)__REV16(top16);
audio_to_uart_buffer[audio_to_uart_wr_ptr + 2*i] = (little_endian_value >> 8) & 0xFF;
audio_to_uart_buffer[audio_to_uart_wr_ptr + 2*i+1] = little_endian_value & 0xFF;
top16 = 0;
}
audio_to_uart_wr_ptr += buffer_size/2;
if(audio_to_uart_wr_ptr >= main_buffer_size){
audio_to_uart_wr_ptr = 0;
}
if(audio_to_uart_data_behind<20) audio_to_uart_data_behind++;
if(uart_tx_state == 0){
send_audio();
}
}
2023-04-13 12:54 AM
how you send/get data from mobile ? usb-> CDC device?
is there a way to "sync" to the data? (like word-clk in I2S)
+
noise in received 16b : if no "volume" multiplication, just as coming in, is there noise also?
2023-04-13 11:24 AM
Via uart, with dma as well. There is zero noise with no multiplication
2023-04-13 12:24 PM
so obviously something around your "volume" multiplication is wrong.
pointer -cast , shift, endianess , swap hi / lo byte ... whatever.
2023-04-18 2:10 AM
and ??
2023-04-18 3:55 AM
I tried changing the byte swap but nothing fixed it. I left it alone got now. It works good enough and I do not have much time. Thank you for your help.