2016-03-10 1:36 AM
Hello ,
I want to configure I2s full duplex mode for Audio Codec with SPI3 module. As per Manual, if I2S module is in Master TX mode , I2Sext module would be in Slave Rx mode . Now my audio codec has been configured as Slave device because of this I2Sext_SD which is RX line is not receiving any data . Can I config I2S & I2Sext in Master TX and Master Rx mode ?? Is there any other way work-around in this scenario ? - Pinkesh #i2s #discovery #stm32f4