2023-11-27 11:40 AM
I have an STM32H563 communicating on I2C4 @ 1 MHz (fast-mode plus) to an I/O expander with no problem. However when I add a temp sensor (TI TMP175) to the same bus, communication doesn't work for the TMP175. The TMP175 communicates > 400 KHz only if a master code is tx following Start condition and before device address. Does the HAL interface support such a master code?
2024-03-27 5:49 AM
Hello @mccabehm ,
Make sure that you are using the correct address.
Use an oscilloscope to check SDA and SCL behavior.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.