2019-08-05 11:49 AM
For some reason I cannot flash my Nucleo (STM32F446) board anymore. It used to work well... I got the following message:
openocd -f ./cfg/openocd.cfg -c "program ./build/ch.elf verify reset" -c "shutdown"
Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 2000 kHz
adapter_nsrst_delay: 100
none separate
Info : Unable to match requested speed 2000 kHz, using 1800 kHz
Info : Unable to match requested speed 2000 kHz, using 1800 kHz
Info : clock speed 1800 kHz
Info : STLINK v2 JTAG v34 API v2 SWIM v25 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.247800
Error: init mode failed (unable to connect to the target)
in procedure 'program'
in procedure 'init' called at file "embedded:startup.tcl", line 506
in procedure 'ocd_bouncer'
** OpenOCD init failed **
shutdown command invoked
Makefile:210: recipe for target 'flash' failed
make: *** [flash] Error 1
Also when I am issuing:
telnet localhost 4444
I get:
Trying 127.0.0.1...
telnet: Unable to connect to remote host: Connection refused
When I plug my Nucleo board I can see its build version etc. Strange.
2019-08-05 12:05 PM
Try strapping BOOT0 high.