cancel
Showing results for 
Search instead for 
Did you mean: 

I want to generate phase shifted PWM for 3 channels in Timer 1 of STM32G474.

Sairaj1987
Associate II

I want to generate phase shifted PWM for 3 channels of Timer 1 of STM32G474.

How to generate, please let me know?

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
waclawek.jan
Super User

Read the Asymmetric PWM mode subchapter of TIM chapter in Reference Manual (RM).

JW

Sairaj1987
Associate II

Hello Waclawek,

Thanks for sharing info. could you please share some example code so as to enable me to proceed further.

Thanks in advance.

ChahinezC
Lead

Hello @Sairaj1987​,

I recommend you checking the "TIM_PWMOutput" example developed on the NUCLEO-G474RE board from the STM32CubeG4. It will certainly help you with your request, you can download the it from the ST official website or through the GitHub repository.

The example is under the following root: "STM32Cube\Repository\STM32Cube_FW_G4_V.XX\Projects\NUCLEO-G474RE\Examples\TIM\TIM_PWMOutput".

I hope my answer has helped you, please mark it as best by clicking on the "Select as Best" button if it fully answered your question. This will help other users find this solution faster.

Thank you.

Chahinez.

Sairaj1987
Associate II

Hello ChahinezC ,

Thank you.

The given example shows to generate 4 PWM signals under one timer i.e. TIM1. My application is to generate the same with phase shift of 60 degrees between each channel.

i.e. Channel 1 : 0 Degree

Channel 2: 60 degree

Channel 3 120 degree

Channel 4 180 degree

So, my obstacle is to provide phase shift between each channel under same timer i.e. TIM1.

Thank you

Sairaj

ChahinezC
Lead

Hello @Sairaj1987​,

Based on the readme file, the example provided is based on Timer1 with the following :

TIM1 Channel1 duty cycle = 50%

TIM1 Channel2 duty cycle = 37.5%

TIM1 Channel3 duty cycle = 25%

TIM1 Channel4 duty cycle = 12.5%

Thank you.

Chahinez.

Sairaj1987
Associate II

Hello ChahinezC ,

I agree with the duty cycle. But all the channels will start at 0 degree whereas, My application is to provide phase shift between all the channels.

Thanks

Sairaj

KnarfB
Super User

3 phases PWM output seems not possible with 1 timer, see https://community.st.com/s/question/0D53W00000esa2XSAQ/is-it-possible-to-create-120-degrees-3-phase-shifted-pwm-with-controllable-duty-cycle try synchronizing 2 timers.

hth

KnarfB

waclawek.jan
Super User

Hi @KnarfB​ ,

> 3 phases PWM output seems not possible with 1 timer

That thread deals with 'F303. The 'G4 have a new and shiny TIM, which has Asynchronous mode and also provision to combine CH5 with some of the other channels (which is obviously an afterthough so is set up differently than Asynchronous mode.

I haven't tried personally but I am confident that 3 different phases are possible in 'G4's TIM1. For 4th phase, indeed, a different timer has to be used, through the master-slave synchronization.

JW