cancel
Showing results for 
Search instead for 
Did you mean: 

I need help getting signal data

OAdem
Associate II

Hi,

I need help getting signal data from EVB with BG96 module using STM32L476RG MCU.

4 REPLIES 4

What kind of help?

Paid help?

What are people supposed to do to help you get L073 code running on the L476? You've provided no code to review, or analysis of what's "not working"

Is this a NUCLEO board?

Perhaps get a native project working on the board, then port back in the L073 code a bit at a time. Watch for things like different USART, different pin utilization, and mux settings.

https://community.st.com/s/question/0D50X00009vMToNSAW/stm32l476-interconnection-with-ecv-with-bg96-module

https://community.st.com/s/feed/0D50X00009vMRDHSA4

https://community.st.com/s/question/0D50X00009vMQHrSAO/stm32l476rg-mcu-not-powering-evb-with-bg96

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
OAdem
Associate II

I am working on NB IOT project to get signal strength of a sim of a mobile operator using EVB BG96 module and STM32L476RG microcontroller. I have a code which was supposed to turn the module on, initialised it and get data to cumulocity cloud but the module fails to power on. Attached with is message is the code for STM32L476RG and EVB board with BG96 module. I am using keil IDE.

Thank you.

I have deleted the duplicates. @OAdem​ if you post multiple times in different place this creates a mess in the community with

  1. others who help making duplicate effort
  2. some threads then may have an answer and others not = hard for others in future to find/learn what the result is