I have two devices. Need to setup UART communication?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-22 6:41 AM
I have two STM32 devices and both are identical, send and receive messages in frame formats. They both have UART, DMA, NVIC etc.
And I need a good strategy to setup a lossless communication between them. There is too much information online, but very little about which is good method. Also this project is configured with RTOS.
What I found online:
--> Interrupts is bad strategy.
--> DMA is the good one, DMA with circular buffer is also a good one.
--> byte format is not reliable, so use frame type.(identifier, address, data, crc)
can someone help me here? I'm actually overwhelmed by these concepts.
Solved! Go to Solution.
- Labels:
-
DMA
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-22 11:12 PM
Honestly seem to be over thinking this. A simple interrupt method should work to prove the method. Then implement DMA TX, if that improves efficiency.
Does the packet form provide for synchronization or integrity checking?
Have you reviewed protocols like SLIP and XMODEM? Or say packet methods used by sensors or GNSS receivers.
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
2022-08-22 6:49 AM
There is no info because your question is still too vage, you still need to make some arquitecture design decisions.
Some examples:
- Which two devices specifically?
- How far are they?
- How fast does the communication need to be?(bytes per second)
- What latency are you able to tolerate?(miliseconds? miroseconds?)
- How realiable does this communication need to be?
- How much RAM/Flash cold you spare for this?
- How many tasks are you running, is your RTOS already pretty busy?
- Do you want to integrate this protocol with an already existing tools/devices echosystem? (for example MAVLINK)
- How experienced is the developer, how much time do you have?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-22 7:06 AM
- Which two devices specifically?
- STM32L431CC
- How far are they?
- less than 3cm.
- How fast does the communication need to be?(bytes per second)
- 9600bps
- What latency are you able to tolerate?(miliseconds? miroseconds?)
- microseconds
- How realiable does this communication need to be?
- Highly reliable. There shouldn't be any loss. (they communicate information, in 14 byte telegrams - send and receive)
- How much RAM/Flash cold you spare for this?
- I have 1MB of RAM, so quite a lot, but no specific number
- How many tasks are you running, is your RTOS already pretty busy?
- Two tasks are running. This communication task should be third one, and no its not busy.
- Do you want to integrate this protocol with an already existing tools/devices echosystem? (for example MAVLINK)
- Nope.
- How experienced is the developer, how much time do you have?
- I have 2 years, but I have 2 month of time. Can be extended upon asking.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-22 11:12 PM
Honestly seem to be over thinking this. A simple interrupt method should work to prove the method. Then implement DMA TX, if that improves efficiency.
Does the packet form provide for synchronization or integrity checking?
Have you reviewed protocols like SLIP and XMODEM? Or say packet methods used by sensors or GNSS receivers.
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
2022-08-23 4:33 AM
True, but this implementation will be used for many things. I want to have some references where I can properly implement this module.
I don't know SLIP but I looked at XMODEM.