cancel
Showing results for 
Search instead for 
Did you mean: 

I have a two dimensional array char as str[2][10].

cjaya.1
Associate II
 I have assigned the string into the char array as "example\n". How do I put the "\n" character in front of the "example\n". I wanted like this "\nexample\n" on the char array

1 REPLY 1
Karl Yamashita
Lead II
#include "string.h"
 
memmove(str[0]+1, str[0], strlen(str[0]));
str[0][0] = '\n';

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.