cancel
Showing results for 
Search instead for 
Did you mean: 

I have a question about the STM32H743...

damon kutten
Associate II

If this device is powered-down (i..e voltage is 0 on all rails), what impedance will be presented by the Port pins? If a pin from a powered-down STM32H743 is connected to a pin on another (fully powered) device, what current drain will occur?

11 REPLIES 11

The answer by @prain here is incorrect. You should mark Uwe Bonnes's answer as the right one.

If you feel a post has answered your question, please click "Accept as Solution".
damon kutten
Associate II

To TDK:

Yes, Uwe Bonnes' answer is correct.

This was confirmed by the 10Kohm series resistor measurement that you took.

I am interested in any additional data you could obtain by using a 100Kohm resistor or 1Mohm resistor in place of the 10Kohm resistor.