2021-01-04 2:24 AM
I'm trying to set up a BDMA Stream with Lptim5 as trigger source. Which interrupt on the Lptim5 can i use? "Lptim5_ait" is not listed as an interrupt in the Lptim section of the manual ( page 1881, table 350).
Happy new year and thanks in advance!
2021-01-04 6:54 AM
Hello @Willi Färber,
lptim_ait is the lptim asynchronous interrupt or what we can call wakeup signal.
it is equivalent to synchronous IT (but mainly used to wakeup the system where all clocks are off).
Imen