cancel
Showing results for 
Search instead for 
Did you mean: 

I generate a flm file, but failed when use this flm to download external flash.

sheng yang
Associate III

I made  a project on keil with generate flm file to download to external flash with my board. My board has a stm32h7b0zbt6 chip with ospi interface with a spi nor flash W25Q128. the interface releate is:

 

 

PF6 ------> OCTOSPIM_P1_IO3
PF7 ------> OCTOSPIM_P1_IO2
PF9 ------> OCTOSPIM_P1_IO1
PB2 ------> OCTOSPIM_P1_CLK
PD11 ------> OCTOSPIM_P1_IO0
PC11 ------> OCTOSPIM_P1_NCS

 

 

and I append the project , is there anyone can help me to check the project ? 

When I try to use this flm file to download code on keil, I get errors like below:

shengyang_0-1734621698216.png

 

0 REPLIES 0