2025-05-21 2:10 PM
I was wondering if anyone had managed to get the LoRaWAN End-Node example running on other MCUs than the STM32L series. I've been trying to get it to run on the STM32U5A9 combined with an SX1262, but I haven't had any luck. I'm trying to integrate this into a clean project structure, unlike the one from the example applications where there are files like sys_app.c that manually configure the SPI bus instead of using CubeMX generated code.
I have manged to succesfully port the SX1262 driver code from Semtech itself (https://github.com/Lora-net/sx126x_driver), however I don't see how to integrate this with the LoRaWAN example.
If anyone has succeeded or has any tips, any help would be appreciated!