cancel
Showing results for 
Search instead for 
Did you mean: 

i can't see CM3 folder in CMSIS folder please help me

chauvoluuhuong
Associate II
Posted on April 23, 2015 at 10:03

apparently to this link https://www.youtube.com/watch?v=_QXoTNP9GIw to write code for SM32F3VC 

i download standard library for st ( CMSIS ) right here http://www.st.com/web/en/catalog/tools/PF258144

and try to find core_cm3.c in  CM3 folder but i cant find it in CMSIS folder that i downloaded  even thought i tried to very times which many have CMSIS folder 

please help me hizzzz !!!!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on April 24, 2015 at 15:08

Hi,

STM32F3 is based on Cortex-M4 with FPU core.

core_cm4.h has to be used for F3, and it is available in the CMSIS package.

If it is missed, this should be an issue with downloaded package (lack of space...).

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.